Tool qualification of Codewarrior V11.1 and FreeMaster 3.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tool qualification of Codewarrior V11.1 and FreeMaster 3.1

ソリューションへジャンプ
1,618件の閲覧回数
magniv-co
Contributor I

We are developing a MCU( S12ZVML) and need to prove tool qualification of Codewarrior v11.1& FreeMASTER3.1.  As I know, there is no certification but I heard that NXP provide customers proven in use documents instead so we try to explain "Increased confidence from use" for qualification. Can I receive the customers proven in use documents?

0 件の賞賛
返信
1 解決策
1,576件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

I sent you CW11.1 Proven In Use document via email.

There is no such document for FreeMaster as this is just a monitoring or debugging tool.

Proven In Use is only required for tools that affect and can change the embedded code or processor.

 

Best regards,

Daniel

元の投稿で解決策を見る

2 返答(返信)
1,558件の閲覧回数
magniv-co
Contributor I

I really appreciate your reply. It was very helpful to me

In case of FreeMASTER, I have to find another method to prove qualification. but it's ok

thank you~ So! much!

0 件の賞賛
返信
1,577件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

I sent you CW11.1 Proven In Use document via email.

There is no such document for FreeMaster as this is just a monitoring or debugging tool.

Proven In Use is only required for tools that affect and can change the embedded code or processor.

 

Best regards,

Daniel