The Usage of MC9S12ZVML's flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The Usage of MC9S12ZVML's flash

ソリューションへジャンプ
1,128件の閲覧回数
xiaofangu
Contributor III

Hello,

   Our product's mcu is mc9s12zvml128,and according to the datasheet,its flash range is from 0xfe0000  to 0xffffff.Recently,we want to change the mcu to mc9s12zvml32,and its flash range is 0xff8000 t0 0xffffff.But I find that my code can still be download to 0xfe0000~0xff7ffff.

   What's wrong with this?

Best Regards!

0 件の賞賛
返信
1 解決策
1,003件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi xiaofangu,

Nothing is wrong. The devices have the same mask set, but not defined peripherals/memory spaces on the MC9S12ZVML32 device are not tested.

If you use peripheral or memory which is not introduced for given device in the datasheet NXP does not guarantee quality of the device. It is on your responsibility

So, please follow the memory ranges which are defined in the datasheet for given device.

Best regards,

Diana

元の投稿で解決策を見る

1 返信
1,004件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi xiaofangu,

Nothing is wrong. The devices have the same mask set, but not defined peripherals/memory spaces on the MC9S12ZVML32 device are not tested.

If you use peripheral or memory which is not introduced for given device in the datasheet NXP does not guarantee quality of the device. It is on your responsibility

So, please follow the memory ranges which are defined in the datasheet for given device.

Best regards,

Diana