The Usage of MC9S12ZVML's flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The Usage of MC9S12ZVML's flash

跳至解决方案
1,109 次查看
xiaofangu
Contributor III

Hello,

   Our product's mcu is mc9s12zvml128,and according to the datasheet,its flash range is from 0xfe0000  to 0xffffff.Recently,we want to change the mcu to mc9s12zvml32,and its flash range is 0xff8000 t0 0xffffff.But I find that my code can still be download to 0xfe0000~0xff7ffff.

   What's wrong with this?

Best Regards!

0 项奖励
回复
1 解答
984 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi xiaofangu,

Nothing is wrong. The devices have the same mask set, but not defined peripherals/memory spaces on the MC9S12ZVML32 device are not tested.

If you use peripheral or memory which is not introduced for given device in the datasheet NXP does not guarantee quality of the device. It is on your responsibility

So, please follow the memory ranges which are defined in the datasheet for given device.

Best regards,

Diana

在原帖中查看解决方案

1 回复
985 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi xiaofangu,

Nothing is wrong. The devices have the same mask set, but not defined peripherals/memory spaces on the MC9S12ZVML32 device are not tested.

If you use peripheral or memory which is not introduced for given device in the datasheet NXP does not guarantee quality of the device. It is on your responsibility

So, please follow the memory ranges which are defined in the datasheet for given device.

Best regards,

Diana