The PS2 pin of s912zvml64 cannot be output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The PS2 pin of s912zvml64 cannot be output

Jump to solution
3,202 Views
maxxu
Contributor IV

Hi

   I found a problem during debugging。The PS2 pin of s912zvml64 cannot be output

I use the following settings

   DDRS_DDRS2 = 1;

   DDRS_DDRS3 = 1;

   DDRS_DDRS4 = 1;

   PS3,PS4 Can output normally,But,PS2,The output is always out of control, and I / O seems to be in the input state all the time

  When I set these three I / O to the input mode, the function of reading Hall signal is normal. In another project, I use these three I / O for output. As a result, only PS3 and PS4 can be controlled. It's really strange

  

0 Kudos
Reply
1 Solution
3,175 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

Possible issues:

1) There is something connected to the pin externally what influences value at the pin
2) There is alternative function enabled and routed to the pin. For example RxD of the SCI. If alternative function(s) is enabled at the pin ten the function with highest priority takes precedence and controls the pin.
3) Somewhere in you SW you accidentaly change the direction of the pin.
4) The pin is destroyed (check behavior with simplified SW on another board)

Best regards,.
Ladislav

View solution in original post

0 Kudos
Reply
4 Replies
3,176 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

Possible issues:

1) There is something connected to the pin externally what influences value at the pin
2) There is alternative function enabled and routed to the pin. For example RxD of the SCI. If alternative function(s) is enabled at the pin ten the function with highest priority takes precedence and controls the pin.
3) Somewhere in you SW you accidentaly change the direction of the pin.
4) The pin is destroyed (check behavior with simplified SW on another board)

Best regards,.
Ladislav

0 Kudos
Reply
3,167 Views
maxxu
Contributor IV

YES,Problem found, MODRR0 was accidentally set,thank you.

Tags (1)
0 Kudos
Reply
3,191 Views
aaronlee
Contributor V

Hi,

 

	DDRS_DDRS2 = 1;		// Set PS2 as Output
  	for(;;)
  	{
		PTS_PTS2 = 1;				// Set PS2 to High
  		Cpu_Delay100US(5000);		// Delay 500ms
		PTS_PTS2 = 0;				// Set PS2 to Low
  		Cpu_Delay100US(5000);		// Delay 500ms
  	}

 

Best Regards,

Aaron

0 Kudos
Reply
3,182 Views
maxxu
Contributor IV

As you said, PS2, PS3 and PS4 are configured in this way, but PS2 cannot be controlled, while PS3 and PS4 are normal

0 Kudos
Reply