The MOSFETs used by the S12ZVML-MINIBRD Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The MOSFETs used by the S12ZVML-MINIBRD Board

跳至解决方案
911 次查看
519315342
Contributor I

S12ZVML-MINIBRD Board use of MOSFETs is the picture 2, while the S12ZVML-MINIBRD_UM.PDF is written in picture 1. The two MOSFETs is the same? And what the type of the MOSFET in Picture 2 , what company?

标签 (1)
0 项奖励
1 解答
756 次查看
iggi
NXP Employee
NXP Employee

Hi,

well, yes there is a difference between transistor specified in the user manual and the one placed on the board, but generally, different is manufacturer.

From the operational point of view, both are very much the same: 30V N-Channel Power MOSFETs. And both are automotive qualified (AEC-Q101).

(usually this happens during manufacturing process of a PCB when some components are exhausted and then alternative part is used as a replacement.)

The manufacturer is for example Vishay:

http://www.vishay.com/docs/68634/sqd50n03.pdf

Regards,

iggi

在原帖中查看解决方案

0 项奖励
3 回复数
756 次查看
519315342
Contributor I

oh,thank you very much !

Can you tell me the models of the MOSFETs in picture 2 ?

0 项奖励
756 次查看
iggi
NXP Employee
NXP Employee

The one from the picture 2 is product of Siliconix, a company which was acquired by Vishai in 1998.

0 项奖励
757 次查看
iggi
NXP Employee
NXP Employee

Hi,

well, yes there is a difference between transistor specified in the user manual and the one placed on the board, but generally, different is manufacturer.

From the operational point of view, both are very much the same: 30V N-Channel Power MOSFETs. And both are automotive qualified (AEC-Q101).

(usually this happens during manufacturing process of a PCB when some components are exhausted and then alternative part is used as a replacement.)

The manufacturer is for example Vishay:

http://www.vishay.com/docs/68634/sqd50n03.pdf

Regards,

iggi

0 项奖励