The MOSFETs used by the S12ZVML-MINIBRD Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The MOSFETs used by the S12ZVML-MINIBRD Board

Jump to solution
1,296 Views
519315342
Contributor I

S12ZVML-MINIBRD Board use of MOSFETs is the picture 2, while the S12ZVML-MINIBRD_UM.PDF is written in picture 1. The two MOSFETs is the same? And what the type of the MOSFET in Picture 2 , what company?

Labels (1)
0 Kudos
Reply
1 Solution
1,141 Views
iggi
NXP Employee
NXP Employee

Hi,

well, yes there is a difference between transistor specified in the user manual and the one placed on the board, but generally, different is manufacturer.

From the operational point of view, both are very much the same: 30V N-Channel Power MOSFETs. And both are automotive qualified (AEC-Q101).

(usually this happens during manufacturing process of a PCB when some components are exhausted and then alternative part is used as a replacement.)

The manufacturer is for example Vishay:

http://www.vishay.com/docs/68634/sqd50n03.pdf

Regards,

iggi

View solution in original post

0 Kudos
Reply
3 Replies
1,141 Views
519315342
Contributor I

oh,thank you very much !

Can you tell me the models of the MOSFETs in picture 2 ?

0 Kudos
Reply
1,141 Views
iggi
NXP Employee
NXP Employee

The one from the picture 2 is product of Siliconix, a company which was acquired by Vishai in 1998.

0 Kudos
Reply
1,142 Views
iggi
NXP Employee
NXP Employee

Hi,

well, yes there is a difference between transistor specified in the user manual and the one placed on the board, but generally, different is manufacturer.

From the operational point of view, both are very much the same: 30V N-Channel Power MOSFETs. And both are automotive qualified (AEC-Q101).

(usually this happens during manufacturing process of a PCB when some components are exhausted and then alternative part is used as a replacement.)

The manufacturer is for example Vishay:

http://www.vishay.com/docs/68634/sqd50n03.pdf

Regards,

iggi

0 Kudos
Reply