Sharing I/O and External Bus using Processor Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sharing I/O and External Bus using Processor Expert

3,162 次查看
ETCTim
Contributor I
Hello,
I am using the 56F8346 DSP. I want to use A0 thru A10 as the address bus, and then use the remaining A pins as GPIO.
 
Can I set this up in PE? When I turn on the address bus, PE conflicts with the BitIO beans that I setup for the remaining pins. Can I tell PE that I only want to use certain address and data lines for the external bus?
 
Thanks,
Tim
 
标签 (1)
0 项奖励
回复
2 回复数

956 次查看
ProcessorExpert
Senior Contributor III
The current version of Processor Expert allows only to enable/disable the whole external bus. However, this feautre has already been implemented into the next upcoming version of Processor Expert.
 
best regards
Petr Hradsky
Processor Expert Support Team
UNIS
0 项奖励
回复

956 次查看
imajeff
Contributor III
If it's like the MC9S12, you could only configure the port as GPIO (then bitbang it), or configure the whole port to be an address bus (expanded i/o).
0 项奖励
回复