Serial monitor for NE64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial monitor for NE64

2,604 Views
MarcV
Contributor I
Hi all,
I erased the serial monitor inside my DEMO9S12NE64 while playing with it using the P&E ICD. Bus as I would like to start using the GNU compiler I would like to reprogram the serial monitor. It is available on-line as AN2548 but this program requires the correct settings for the NE64 and those are not explicitly in there (file S12SerMon2r1.def) even though the version description states that support for the NE64 was added.
I know the NE64 runs at 25MHz and the switch is connected to PTG4 so I can use these settings, but I don't know which of the memory settings to uncomment.
Can anyone help?
Thanks in advance - Marc
Labels (1)
0 Kudos
Reply
1 Reply

1,003 Views
Ilocano
Contributor I
Below are settings we used for the NE64 Serial monitor. See it helps you.

The un-commented portions are for the NE64
See links for other docs if they are of use too.

http://support.technologicalarts.ca/docs/
http://support.technologicalarts.ca/docs/Adapt9S12NE/
http://support.technologicalarts.ca/docs/neCore12/

;*********************************************************************
;* One device specific NVM definition below should be uncommented
;*********************************************************************
Dx512:
;EEpromStart: equ $0400 ;eeprom start
;EEpromEnd: equ $07FF ;eeprom end (rest is hidden)
;RamStart: equ $0800 ;first RAM location
;SectorSize: equ $0400 ;Flash sector size
;FlashBlks: equ $04 ;# of flash blks
;LowestPage: equ $20 ;lowest page
;PagesBlk: equ $08 ;pages per block
;softwareID4: equ $0400 ;device ID #

Dx256:
;EEpromStart: equ $0400 ;eeprom start
;EEpromEnd: equ $0FFF ;eeprom end
;RamStart: equ $1000 ;first RAM location
;SectorSize: equ $0200 ;Flash sector size
;FlashBlks: equ $04 ;# of flash blks
;LowestPage: equ $30 ;lowest page
;PagesBlk: equ $04 ;pages per block
;softwareID4: equ $0011 ;device ID #

Dx128:
;EEpromStart: equ $0800 ;eeprom start
;EEpromEnd: equ $0FFF ;eeprom end
;RamStart: equ $2000 ;first RAM location
;FlashBlks: equ $02 ;# of flash blks
;SectorSize: equ $0200 ;Flash sector size
;LowestPage: equ $38 ;lowest page
;PagesBlk: equ $04 ;pages per block
;softwareID4: equ $0110 ;device ID #

Dx64:
;EEpromStart: equ $0C00 ;eeprom start
;EEpromEnd: equ $0FFF ;eeprom End
;RamStart: equ $3000 ;first RAM location
;FlashBlks: equ $01 ;# of flash blks
;SectorSize: equ $0200 ;Flash sector size
;LowestPage: equ $3C ;lowest page
;PagesBlk: equ $04 ;pages per block
;softwareID4: equ $0201 ;device ID #

NE64:
EEpromStart: equ $0000 ;eeprom start
EEpromEnd: equ $0000 ;eeprom End
RamStart: equ $2000 ;first RAM location
FlashBlks: equ $01 ;# of flash blks
SectorSize: equ $0200 ;Flash sector size
LowestPage: equ $3C ;lowest page
PagesBlk: equ $04 ;pages per block
softwareID4: equ $8200 ;device ID #


E128:
;EEpromStart: equ $0000 ;eeprom Start (no EEprom)
;EEpromEnd: equ $0000 ;eeprom End
;RamStart: equ $2000 ;first RAM location
;FlashBlks: equ $01 ;# of flash blks
;SectorSize: equ $0400 ;Flash sector size
;LowestPage: equ $38 ;lowest page
;PagesBlk: equ $08 ;pages per block
;softwareID4: equ $5102 ;device ID #

C32:
;EEpromStart: equ $0000 ;eeprom start (no EEprom)
;EEpromEnd: equ $0000 ;eeprom End
;RamStart: equ $3800 ;first RAM location
;FlashBlks: equ $01 ;# of flash blks
;SectorSize: equ $0200 ;Flash sector size
;LowestPage: equ $3E ;lowest page
;PagesBlk: equ $02 ;pages per block
;softwareID4: equ $3300 ;device ID #

Dx32:
;EEpromStart: equ $0C00 ;eeprom start
;EEpromEnd: equ $0FFF ;eeprom End
;RamStart: equ $3800 ;first RAM location
;FlashBlks: equ $01 ;# of flash blks
;SectorSize: equ $0200 ;Flash sector size
;LowestPage: equ $3E ;lowest page
;PagesBlk: equ $02 ;pages per block
;softwareID4: equ $0300 ;device ID #

H256:
;EEpromStart: equ $0400 ;eeprom start
;EEpromEnd: equ $0FFF ;eeprom end
;RamStart: equ $1000 ;first RAM location
;SectorSize: equ $0200 ;Flash sector size
;FlashBlks: equ $04 ;# of flash blks
;LowestPage: equ $30 ;lowest page
;PagesBlk: equ $04 ;pages per block
;softwareID4: equ $1001 ;device ID #

;*********************************************************************
;* One application specific Osc definition below should be uncommented
;* If Additonal eneries are required initSYNR and initREFDV must be
;* set for 24MHz PLL frequency. SCI communication problems will result
;* at other frequencies.
;*********************************************************************
;OscFreq: equ 4000 ;Enter Osc speed
;initSYNR: equ $05 ; mult by synr + 1 = 6 (24MHz)
;initREFDV: equ $00 ;
;---------------------------------------------------------------------
;OscFreq: equ 8000 ;Enter Osc speed
;initSYNR: equ $02 ; mult by synr + 1 = 3 (24MHz)
;initREFDV: equ $00 ;
;---------------------------------------------------------------------
;OscFreq: equ 16000 ;Enter Osc speed
;initSYNR: equ $02 ; mult by synr + 1 = 3/2 (24MHz)
;initREFDV: equ $01 ; divide by Refdiv + 1
;---------------------------------------------------------------------
OscFreq: equ 25000 ;Enter Osc speed
initSYNR: equ $00 ; mult by synr + 1 = 1 (25MHz)
initREFDV: equ $00 ; divide by Refdiv + 1

;*********************************************************************
;* One application specific Run Load Switch definition below should be
;* uncommented. This defininition sets the placement of the switch to
;* force entery into the monitor. The switch sould be configure such
;* that the load position applies a logic zero to the selected pin.
;*********************************************************************
;---------------------------------------------------------------------
;SwPort: equ PTQ ;pushbutton sw connected to port Q
;Switch: equ PTQ0 ;switch connected to PTQ bit-5
;SwPullup: equ PERQ ;pullup enable for sw port
;mSwPullup: equ PTQ0 ;Mask value to enable for sw port
;---------------------------------------------------------------------
;SwPort: equ PTP ;pushbutton sw connected to port P
;Switch: equ PTP5 ;switch connected to PTP bit-5
;SwPullup: equ PERP ;pullup enable for sw port
;mSwPullup: equ PTP5 ;Mask value to enable for sw port
;---------------------------------------------------------------------
;SwPort: equ PORTA ;pushbutton sw connected to port A
;Switch: equ PTA6 ;switch connected to PTA bit-6
;SwPullup: equ PUCR ;pullup enable for sw port
;mSwPullup: equ PUPAE ;Mask value to enable for sw port
;---------------------------------------------------------------------
;SwPort: equ PORTB ;pushbutton sw connected to port B
;Switch: equ PTB4 ;switch connected to PTB bit-4
;Switch: equ PTB0 ;switch connected to PTB bit-0
;SwPullup: equ PUCR ;pullup enable for sw port
;mSwPullup: equ PUPBE ;Mask value to enable for sw port
;---------------------------------------------------------------------
;Adapt9S12NE64
;SwPort: equ PTL ;pushbutton sw connected to port L
;Switch: equ PTL6 ;switch connected to PTL bit-6
;SwPullup: equ PERL ;pullup enable for sw port
;mSwPullup: equ PTL6 ;Mask value to enable for sw port
;---------------------------------------------------------------------
;neCore12M64
SwPort: equ PTL ;pushbutton sw connected to port L
Switch: equ PTL3 ;switch connected to PTL bit-3
SwPullup: equ PERL ;pullup enable for sw port
mSwPullup: equ PTL3 ;Mask value to enable for sw port
;---------------------------------------------------------------------
;SwPort: equ PTP ;pushbutton sw connected to port P
;Switch: equ PTP0 ;switch connected to PTP bit-0
;SwPullup: equ PERP ;pullup enable for sw port
;mSwPullup: equ PTP0 ;Mask value to enable for sw port
;---------------------------------------------------------------------

AllowSci0 equ $1 ;set to one to allow user application
; use of sci0. The monitor will not
; Be able to break into user code if
; this is set. This will effect debugging
0 Kudos
Reply