Serial monitor for 9S12X processors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial monitor for 9S12X processors

1,114 Views
davidvogel
Contributor I

I am using CodeWarrior Development Studio for S12(X) 5.1 for a 9X12XE128 processor.  It appears the serial monitor is not supported on the X processors.  I see an old post that says they are not (yet) supported.  Is that correct or am I doing something wrong?  Any plans if the future?

Labels (1)
0 Kudos
Reply
3 Replies

977 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

we have an4258 for S12(X)

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4258.pdf

here is demo code:

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4258SW.zip

9X12XE128 demo code is also included in the package.

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

977 Views
davidvogel
Contributor I

Thank you, that information is interesting and potentially useful but the question was:  Does CodeWarrior support the serial monitor to the 9S12XE processors and if not, is there any plans to support it.  I presume the answer to both questions is "no" but just wanted to confirm.  Thanks.

0 Kudos
Reply

977 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

CodeWarrior 5.1 is the exact ide that can support 9s12x family well, so 9s12xe is also included.

Best regards.

Jennie

0 Kudos
Reply