Sample makefile of S12ZVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample makefile of S12ZVM

1,331 Views
huuhuynhchi
Contributor III

Dear all,

 

I would like to manage my source to build into executable file (.s19). I used COSMIC compiler but I haven't had any experience about makefile. If you had a sample makefile to manage a big source code, Could you please help me ? I also wrote a makefile for my example code as the attached file and I would like to assign my executable file (.s19) to a specific folder to easily manage. Example: output includes : *.s19, *z12 and *.map and I hope that can put them in a folder different from source folder.

 

Thank all very much!

Original Attachment has been moved to: S12zvm.mak.zip

Original Attachment has been moved to: source.zip

Labels (1)
Tags (3)
1 Reply

1,010 Views
RadekS
NXP Employee
NXP Employee

Hi Huu,

Unfortunately I don't have experiences with COSMIC compiler. However I suppose that there must be some configuration for that.

Did you contacted COSMIC?

http://www.cosmic-software.com/support_form.php


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------