SCI on MC9S12XEQ512 not working without PE micro BDM cable and Hiwave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCI on MC9S12XEQ512 not working without PE micro BDM cable and Hiwave

423件の閲覧回数
dakotabassett
Contributor I

I have encountered a problem while trying to test and SCI module on my micro. It works fine with the BDM cable attached and Hiwave running, it requires both to function. As soon as I disconnect the BDM cable or close hiwave the SCI immediately stops transmitting. I am transmitting from SCI0 to SCI1 every 20 milliseconds.

ラベル(1)
0 件の賞賛
2 返答(返信)

320件の閲覧回数
dakotabassett
Contributor I

Is there any relationship between the two that I am not understanding?

0 件の賞賛

320件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

see answer to the following topic, it is very much the same as to this one:

https://community.freescale.com/thread/352246

Regards,

iggi

0 件の賞賛