S9S12G128F0VLF - Max pin rating for digital pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S9S12G128F0VLF - Max pin rating for digital pins

702件の閲覧回数
Nivetha
Contributor I

Hello Team,

In S9S12G128F0VLF datasheet, absolute max rating of each pin is 6V but I would like to know how much duration micro controller can withstand 6V?

Thanks!

Nivetha

0 件の賞賛
返信
1 返信

687件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

This is not defined. The maximum ratings define a status when the MCU is not damaged but the correct behavior is not guaranteed. The MCU is still able to work correctly after returning to operating conditions. However, you can sometimes meet with note for maximum rating that some parameter has cumulative effect. If it is no mentioned cumulative effect has not to be considered.

Best regards,

Ladislav

0 件の賞賛
返信