where to find drive current of S912ZVML64 HGx and LGx pins,sink current and source current?
Hi,
The concept of the HS drivers is shown in the RM, Section 18.5.1 FET Pre-Driver Details along with some calculations of I_out.
.
The current depends on the selected slew rate (GSRCHS[2:0]).
Table E-1 specifies the HG/LG turn on (turn off) time vs 10nF load at the fastest and slowest slew rate.
Regards,
Daniel
dear danielmartynek
thank you for your answer ,IOUT ~ IREF (R1/R2) k,are the ratio of the transistor sizes of T1 and T2 k=450 and the ratio of the resistors R1/R2=36 fixed ?
IOUTmax = 80uA*36*450 = 1.296 A,eg. VLS = 11 V,Rg_on resistance value shoud more than 11/1.296 = 8.487 ?
Regards
Hello,
The calculation is correct, but it is rather theoretical.
The Turn off / Turn on time at a specific load is specified:
Regards,
Daniel
dear danielmartynek
S12ZVM-EFP Electronical Fuel Pump Reference Design,HD LINE 24Arms 34Apeak,How do I calculate?250W @12V