S912ZVML31F1MKF_Problem_VBSx_Pin_Protect

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912ZVML31F1MKF_Problem_VBSx_Pin_Protect

1,180 Views
danny_li
Contributor II
   1.VBSx Pin of  "S912ZVML31F1MKF" ,  TVS diodes have been added to the pins, The pin is occasionlly damaged,very small probability;
   2.There were other projects before, did the same happen?Can you give me some Suggestions which directions to check?
   3.If I add TVS, do I still need to use Cfilt and Rfilt?
Tags (1)
0 Kudos
Reply
1 Reply

1,107 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello danny.li@weikeng.com.cn,

AC component of voltage peaks on HSx pin can pass through the CBS capacitor to VBSx pin that is internally connected to VCP. The voltage can exceed the maximum ratings and damage the MCU.
Regardless of the TVS diodes, the ringing should be identified using an oscilloscope with proper rating (200 MHz or higher) and differential probes with minimized/compensated loops shall be used.
The optional VBS RC filter can be used to filter the ringing.
I have sent you a presentation that describes the filters.

BR, Daniel

0 Kudos
Reply