S12zvl EEPROM Erase sector time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12zvl EEPROM Erase sector time

ソリューションへジャンプ
1,427件の閲覧回数
charudattaingal
Contributor IV

Dear Team,

 

I am using S12zvl 128 micro, It is taking 5.04ms to erase one sector (4 Bytes) on EEPROM

is there any way to reduce Erase sector time for EEPROM ?

 

Thanks & Regards,

Charudatta

ラベル(1)
0 件の賞賛
返信
1 解決策
1,249件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Charudatta,

Erase sector time for EEPROM cannot be significantly reduced. This time could be slightly influenced by NVM Operating frequency (0.8 .. 1.05MHz) and Bus frequency (1 .. 32MHz) while typical 5.04ms value is calculated for 1MHz fNVMOP and 32MHz fNVMBUS.

Additionally this time could grow during life time due to aging effect. Erase EEPROM sector time grows with number of EEPROM write cycles - that helps extend the endurance capability for the EEPROM.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,250件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Charudatta,

Erase sector time for EEPROM cannot be significantly reduced. This time could be slightly influenced by NVM Operating frequency (0.8 .. 1.05MHz) and Bus frequency (1 .. 32MHz) while typical 5.04ms value is calculated for 1MHz fNVMOP and 32MHz fNVMBUS.

Additionally this time could grow during life time due to aging effect. Erase EEPROM sector time grows with number of EEPROM write cycles - that helps extend the endurance capability for the EEPROM.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信