Hi,
I am using S12ZVM evaluation board (S12ZVMx12EVB), and I am trying to configure PLL clock frequency as 100Mhz so that the Bus frequency will 50HZ.
For this I have set following register value considering crystal of 4MHz-
setReg16(IVBR, 0xFFFEU);
/* Disable the availability of a free-running clock on the ECLK pin. This clock has a fixed rate equivalent to the
* internal bus clock.
* ECLKCTL: NECLK=1,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
setReg8(ECLKCTL, 0x80U);
/* System clock initialization */
/* Procedure proposed by to setup PLL and Oscillator */
/* For OSC = 4 MHz and Bus Clock = 50MHz, That is VCOCLK = 100MHz */
/* Protection of the clock configuration registers from accidental overwrite
* CPMUPROT: ??=0,??=0,??=1,??=0,??=0,??=1,??=1,PROT=0 */
setReg8(CPMUPROT, 0x26U); /* Disable protection of clock configuration registers */
/* As we are using RTI, to do not halt RTI in staop mode we need to use Pseudo Stop Mode.
* CPMUCLKS: PSTP=1 */
clrReg8Bits(CPMUCLKS, 0x40U);
/* System clocks are derived from PLLCLK, fbus = fPLL / 2.
* CPMUCLKS: PLLSEL=1 */
setReg8Bits(CPMUCLKS, 0x80U); /* Enable the PLL to allow write to divider registers */
/* PLL Clock = 100 MHz, divide by one *
* If PLL is locked (LOCK=1),fPLL = fVCO/(POSTDIV + 1)
* Here, fPLL = fVCO
* CPMUPOSTDIV: ??=0,??=0,??=0,POSTDIV4=0,POSTDIV3=0,POSTDIV2=0,POSTDIV1=0,POSTDIV0=0 */
setReg8(CPMUPOSTDIV, 0x00U); /* Set the post divider register */
/* Whenever changing PLL reference clock (REFCLK) frequency to a higher value
* it is recommended to write CPMUSYNR = 0x00 in order to stay within specified
* maximum frequency of the MCU
* CPMUSYNR: VCOFRQ1=0,VCOFRQ0=0,SYNDIV5=0,SYNDIV4=0,SYNDIV3=0,SYNDIV2=0,SYNDIV1=0,SYNDIV0=0 */
setReg8(CPMUSYNR, 0x00U); /* Set the multiplier register */
/* configure PLL reference clock (REFCLK) for usage with Oscillator
* OSC = 4MHz divide by 2 (1+1) = 2 MHz, REFCLK range 1MHz to 2 MHz (REFFRQ[1:0] = 00)
* CPMUREFDIV: REFFRQ1=0,REFFRQ0=0,??=0,??=0,REFDIV3=0,REFDIV2=1,REFDIV1=1,REFDIV0=1 */
setReg8(CPMUREFDIV, 0x01U); /* Set the divider register */
/* enabled oscillator clock monitor reset
* It must be done before setting OSCE bit in CPMUOSC register
* CPMUOSC2: ??=0,??=0,??=0,??=0,??=0,??=0,OMRE=1,OSCMOD=0 */
setReg8(CPMUOSC2, 0x02U); /* Configure external oscillator options */
/* enable external Oscillator, switch PLL reference clock (REFCLK) to OSC
* CPMUOSC: OSCE=1,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
setReg8(CPMUOSC, 0x80U); /* Enable the oscillator */
/* CPMUPLL: ??=0,??=0,FM1=0,FM0=0,??=0,??=0,??=0,??=0 */
setReg8(CPMUPLL, 0x00U); /* Set the PLL frequency modulation */
/* multiply REFCLK = 2MHz by 2*(24+1)*2MHz = 100MHz
* VCO range 80 to 100 MHz (VCOFRQ[1:0] = 11)
* SYNDIV = 24
* CPMUSYNR: VCOFRQ1=1,VCOFRQ0=1,SYNDIV5=0,SYNDIV4=1,SYNDIV3=1,SYNDIV2=0,SYNDIV1=0,SYNDIV0=0 */
setReg8(CPMUSYNR, 0xD8U); /* Set the multiplier register */
/* Check The oscillator is qualified by the PLL*/
while(CPMUIFLG_UPOSC == 0U) { /* Wait until the oscillator is qualified by the PLL */
}
But with this configuration Controller getting hang/going into exception. when I tried to change and configure the fPLL bellow 60Mhz it is working fine.
Please help me to resolve this issue.
Regards,
Amey