S12ZVML Timer0 Interrupt priority

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12ZVML Timer0 Interrupt priority

1,337 次查看
frankkong
Contributor III

Now ,I have a problem. 

I use the interrupt of Timer0 IOC0 (vector address 0x1CC)and IOC3(vector address 0x1C0). IOC3 is for input capture and IOC0 for output compare. The timer base frequency is 200K.  The problem is when I set the different priority it will meet some problem. If I set the same priority it works well. You can see the problem below:

 TIM0TC3 += 500 , cause the problem. What can I do?

   

timer init.pngIOC0 interrupt.pngIOC3 interrupt.png中断优先级.pngTIME0TC3.png

Thanks!

标记 (1)
0 项奖励
回复
3 回复数

1,153 次查看
RadekS
NXP Employee
NXP Employee

Hi Frank,

Just fast hint:

Please do not use commands like TIM0TFLG1_C0F = 1; for flag clearing. This command is translated as read-modify-write command and therefore it will clear all pending interrupt flags instead of only one of them.

Please use commands like TIM0TFLG1 = TIM0TFLG1_C0F_MAP; or TIM0TFLG1 = 0x01; for clearing one flag in your ISR. 

For more details please check our application note AN2554 Clearing and Disabling Interrupt Flags

http://www.nxp.com/files/microcontrollers/doc/app_note/AN2554.pdf


I hope it helps you

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,153 次查看
frankkong
Contributor III

Thanks Radek,

  It works.

Best wish!

0 项奖励
回复

1,153 次查看
RadekS
NXP Employee
NXP Employee

Hi Frank,

Thank you for your note.

I am glad that it works now.

Radek

0 项奖励
回复