Hi,
The correct version of the CodeWarrior can be found at:
It is CodeWarrior® for MCUs (Eclipse IDE)
Evaluation version works like full version for 30 days then, if there is no license, works like special with limitations described at page 3 (column ColdFire, ColdFire+, DSC, Kinetis, MPC55xx MCUs,
PX, RS08, S08 and S12Z) of the document
http://www.nxp.com/assets/documents/data/en/fact-sheets/950-00437.pdf
Opening a project can be dono in following way. The CW10 has the cool feature that you could simply drag the folder with your project and drop it into CodeWarrior Projects window. The CW will import it into the workspace. This way you could import several projects.
The next option is menu-File-Import-General-Existing Projects into Workspace-Select directory with your project(s).
Best regards,
Ladislav
Hi,
I would like to ask you, if it is possible, to communicate in English.
Translation:
Hello, I have already installed this SW(S12ZVML-MINIBRD_BLDC.exe ). Should I open it with CodeWarrior? can you tell me how to open and use it with CW step by step? I use CW6.0. Is this version too low? I use 32bit windows, can you give me a suitable CodeWarrior version link?
Web Translator says:
" I want to download the S12ZVML-MINIBRD_BLDC source program on the official website, but I downloaded the S12ZVML-MINIBRD_BLDC.exe executable file and how this executable file is used. Where is the development board source code downloaded and how can I get the source code for this development board?"