S12ZVML-MINIBRD And FreeMASTER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12ZVML-MINIBRD And FreeMASTER

855 次查看
519315342
Contributor I

Use S12ZVML-MINIBRD to control the motor, use FreeMASTER to control motor speed, Can FreeMASTER change the current limit ? FreeMASTER current can only be transferred to 10A.

标签 (1)
0 项奖励
回复
1 回复

723 次查看
Martin35804
NXP Employee
NXP Employee

Hi,

I assume you use Complete BLDC motor control application software package for S12ZVML-MINIBRD board.:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12ZVML-MINIBRD&fpsp=1&tab=Design_Too...

When you compile the demo and flash it to the miniboard connected with BLDC motor you can start to run the motor from the FreeMaster project and actually you can set DC bus current limit in case the DC bus current that is being filtered and measured can potentially extend this limit. In such case the speed of the motor will be slowed down to prevent any high current.

pastedImage_1.png

0 项奖励
回复