S12ZVM_CAN ISR(Cpu_Interrupt)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVM_CAN ISR(Cpu_Interrupt)

2,632 Views
18647340486
Contributor II

Dear all,

There was a problem when I implemented an interrupt handler. As shown below.

__interrupt void INT_STATUS(void){
 byte Status = CAN0RFLG;              /* Read the status register */
 if((Status & CAN_STATUS_BOFF_MASK) == CAN_STATUS_BOFF_MASK) { /* Bus-Off state */
   ErrFlag |= CAN_STATUS_BOFF_EXT_MASK;
   ErrFlag |= (Status & 0x83U);       /* Add error flags */
 }
 else {
   ErrFlag |= (Status & 0xBFU);       /* Add error flags */
 }
 CAN0RFLG = 0xFEU;                    /* Reset error flags */
 if ((Status & CAN_STATUS_BOFF_MASK) == CAN_STATUS_BOFF_MASK) { /* Is busoff error detected? */
   CAN1_OnBusOff();                   /* If yes then invoke user method */
 }
 CAN0RFLG = CAN0RFLG_CSCIF_MASK;
}
The CPU generated an error interrupt while implementing the above interrupt function.As shown below.
ISR(Cpu_Interrupt)
{
  /*lint -save -e950 Disable MISRA rule (1.1) checking. */
  asm(BGND);
  /*lint -restore Enable MISRA rule (1.1) checking. */
}
I didn't find the problem point.
I need your help.
Thanks.
0 Kudos
Reply
2 Replies

2,374 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

The Processor expert function ISR(Cpu_Interrupt) is called from each unimplemented interrupt to catch the unexpected
event. The example below can be useful to identify the unimplemented interrupt.

S12Z Interrupt catcher for unexpected interrupts 

Could you please check the "3.3.2.2 Error Code Register (MMCECH, MMCECL)"?

Also, in the RM rev. 2.11 in the section "13.3.2.5 MSCAN Receiver Flag Register (CANRFLG)" we can see that RSTAT[1:0] and TSTAT[1:0] flags are read-only.

I hope it helps you.

Best Regards,

Diana

2,374 Views
18647340486
Contributor II

Hi,

This problem has been solved . The reason is that one of interrupts was not complete.Thank you for you help.

Best Regards,

Katherine

0 Kudos
Reply