S12ZVL SCI Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S12ZVL SCI Driver

跳至解决方案
2,925 次查看
charudattaingal
Contributor IV

Requesting basic Uart(SCI) driver example code for S12ZVL Micro.

标签 (1)
1 解答
2,134 次查看
RadekS
NXP Employee
NXP Employee

Hi Charudatta,

I prepared for you simple SCI example code for S12ZVL.

Please look at attached project.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,134 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

I would like only to add.

As an SCI debug console you can use FreeMASTER.

The tool is free and you can use different connections between PC and MCU. (UART, BDM, CAN,...)

The tool provides access to the MCU during run mode, provides you  data visualization, recorder and.....

FreeMASTER Run-Time Debugging Tool|NXP 

Best regards,

Ladislav

0 项奖励
回复
2,135 次查看
RadekS
NXP Employee
NXP Employee

Hi Charudatta,

I prepared for you simple SCI example code for S12ZVL.

Please look at attached project.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------