I am now testing the protection for misplug of our controller with S12ZVC.
On the controller, S12ZVC's output pin, CANH and CANL, of CANPHY is routed to the connector's pin.
One of the test we did is making CANL shorted to 24VDC, the norminal voltage of commerical vehicle.The first two time do not damage the chip and the chip was damaged in the third time. The phenomenon is that the CAN node did not transmit message and the chip heated up quickly while the other function of chip still worked for a while.
The reference manual of CANPHY declares that it is compliant for 12 V battery systems refering to ISO 11898-2 and ISO 11898-5 which needs the voltage bear up to 40V. The Appendix I 'S12CANPHY Electrical Specifications' also declares this electrical characteristics up to 40V.
The process i did this test is:1, switch off the main switch to cut the battery 2, short the CANL pin to the Vin pin with wires 3, switch on the main switch to supply 24VDC at the Vin and GND.
So my question is that do I misunderstand the electrical specification of CANPHY and it can not bear such high voltage? Anything can I do if I want to pass this test.