S12ZVC Problem of simultaneous use of ADC and EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVC Problem of simultaneous use of ADC and EEPROM

810件の閲覧回数
s_kim1
Contributor III

Hello,
I use S12ZVCA19.
I used the sample code to create an ADC input and a PWM output.
I added the sample code of ZVL32-EEPROM-CW106 here to check that EEPROM works.
I would like to write EEPROM when the MCU is running and continue to use ADC after that.
However, after the EEPROM is executed, the ADC cannot read the value.
while (0x00 == ADC0CONIF) {} <- It will stop at this point.
How do I use ADC and EEPROM together?

If you can't use it together, please suggest another method.
I look forward to your answer.
Thank you.

0 件の賞賛
返信
0 返答(返信)