S12ZVC ADC 12bits Resolution with Processor Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S12ZVC ADC 12bits Resolution with Processor Expert

跳至解决方案
1,577 次查看
jinliangsun
Contributor III

I'm working with DEVKIT-S12ZVC board. I use processor expert to configure the ADC module. With PE I can only select  8 bits or 10 bits mode but not 12 bits mode. But according to the reference manual it does support 12 bits mode.

1.4.13 Analog-to-Digital Converter Module (ADC)
• 12-bit resolution
• Up to 16 external channels and 8 internal channels
• Left or right aligned result data

...

Is it possible to use 12 bits mode with Processor Expert generated code? 

Thanks,

Bruce

0 项奖励
回复
1 解答
1,368 次查看
kef2
Senior Contributor V

Hi,

9S12ZVC - 10bit ADC, 9S12ZVCA - 12bit ADC. Did you select non -A derivative?

Edward

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,368 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi jinliangsun,

The Edward is right. When you creating the project you need to choose the variant of MCU S12ZVCA192 (in the case you are using DEVKIT-S12ZVC development platform for S12ZVC|NXP) as you can see below:

pastedImage_53.png

After that, you can select 12bit ADC.

I hope it helps you and thanks, Edward.

Best regards,

Diana

1,367 次查看
jinliangsun
Contributor III

Hi Diana,

Thanks for your response. I did select the wrong derivarative.

Regards,

Bruce

0 项奖励
回复
1,369 次查看
kef2
Senior Contributor V

Hi,

9S12ZVC - 10bit ADC, 9S12ZVCA - 12bit ADC. Did you select non -A derivative?

Edward

0 项奖励
回复