S12XD document for EEprom programming (S12EETX4KV0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12XD document for EEprom programming (S12EETX4KV0)

2,041 次查看
Bee
Contributor III
This may be obvious to some of you, but I can't understand the timing setting of the second example on page 25, using Figure 4-1. The osc. clk is 16 MHz and the Bus clk is 40 Mhz (Tbus=0.025 usec). I get EDIV[5:0]=10 and they get EDIV[5:0]=50. And if I used an osc. clk of 15 MHz, I would get and EDIV[5:0]=5. Where am I going wrong?
标签 (1)
0 项奖励
回复
2 回复数

920 次查看
Lundin
Senior Contributor IV
Who are "they"? I quote the EEPROM datasheet:

"If the oscillator clock frequency is 16 MHz and the bus clock frequency is 40 MHz, ECLKDIV bits EDIV[5:0] should be set to 0x0A (001010) and bit PRDIV8 set to 1."

You calculation for 15MHz seems to be wrong though, you should get the value INT(9.42) = 9.
0 项奖励
回复

920 次查看
Bee
Contributor III
Thanks for your reply. "They" are the writers of the EEprom document (S12EETX4KV0). Apparently we have different versions. Even my Flash programming document has the same example:
"If the oscillator clock frequency is 16MHz and the bus clock frequency is 40MHz, FCLKDIV bits FDIV[5:0] should be set to "50" (110010) and bit PRDIV8 set to "1". The resulting FCLK frequency is then 182kHz."

So the document must have been corrected and I am out of date.

Thank you also for correcting my 15 MHz example.
0 项奖励
回复