Hi All,
I m trying to read the page 0x00780000 to 0x00783FFF ( global Address ) and calculate the CRC16 of the flash memory
#define FLASH_START_ADDR 0x00780000 #define FLASH_END_ADDR 0x00783FFF
the function calculate every 64 bytes the crc and go out from the function again
void Flash_CalcCRC(void) { // Puffer Zeiger auf aktuelles Byte mit Startadresse initialisieren static T_UC08* pucBuffer = (T_UC08*) FLASH_START_ADDR; // <-- wrong content // berechne nur ein Teil des Flashes T_UI16 uiBytesCounter = 0; // Temporäre Variable T_UI16 uiCryptPos = 0; // nur eine gewisse Anzahl an Byte berechnen und die Funktion wieder verlassen for (ulNumLoops ; (ulNumLoops <= FLASH_END_ADDR) && (uiBytesCounter < 64 ); ulNumLoops++) { // Bytes Zähler inkrementieren uiBytesCounter++; // Word aus Puffer in uiCryptPos kopieren uiCryptPos = (T_UI16) *pucBuffer; // also wrong // Pufferzeiger inkrementieren pucBuffer++; // EXOR mit RückgabeCRC uiCryptPos ^= uiFlashCRC16; // CryptArrays einrechnen uiFlashCRC16 = *(T_UI16*)(uiCRC16l + (uiCryptPos & 0x000F)) ^ *(T_UI16*)(uiCRC16h + ((uiCryptPos & 0x00F0) >> 4)) ^ (uiFlashCRC16 >> 8); } if ( ulNumLoops == FLASH_END_ADDR ) { ucFinishFlag = 1; Flash_SetCRC16(uiFlashCRC16); } }
MY PROBLEM is, when I try to read the flash memory, see uiCryptPos or *pucBuffer, in the debug modus, the content of memory is wrong!
My function works very good, when I calculate the page at start address 0x007F4000 to 0x007F7FFF
I dont know what to do and there is no help in the web concerning my problem.
thanks for help in advance
best regards
Solved! Go to Solution.
Hi,
global addresses in Cosmic require the modifier @gpage, you can try something like this:
/* gpage pointer allows accessing any area of global map, paged and non paged */
@far @gpage unsigned int uiMP @0x00FB8000;
@far @gpage unsigned int *puiMP;
*puiMP = &uiMP;
while (puiMP < (@far @gpage unsigned int*) 0x00FBBFFF)
{
uiCryptPos = *puiMP;
/* Here you calculate your CRC and then increment the pointer */
puiMP ++;
}
I hope it works.
Hello
if the address you specify is a global address you need to define and cast the pointer as a far pointer.
static T_UC08 *far pucBuffer = (T_UC08 *far) FLASH_START_ADDR;
This should work better
CrasyCat
hello CarsyCat,
thanks for reply, I change it but It doesnt wor, now I get the content of the address 4000
While creating the S19 File, I get the error
S2060F800000006AError:(9) S-Record Data Not In Specified Memory Map
maybe the is something wrong with the address F80000
I dont really know
another question, what about if I m working with the pages address E08000 - E0BFFF
thanks a lot for the answer
Hm, with CraseCat suggestion my CW5.0 copy properly reads from global 0x780000.
What tool gives you error about S-Record not in specified memory map? Is it Sreccvt?
Don't understand you question about paged (logical) E08000. Do you want to read data from there? Then convert paged E08000 to global as E0*4000 + 8000-8000 + 400000 = 780000
where *4000 is mul by page size
-8000 is remove page window ofset
+400000 - start of PPAGE-memory in global memory map
Hi Kef, Hi CrasyCat,
first thanks so much for your answer!!!
to Kef:
I m working with the cosmic Compiler Ver 4.7.10 and the codewarior debugger with the IndartOne
the s19 File is creating with the SRecCvt v1.0.26 and the command in the Makefile is:
$(SRECCVT) -gmb 400000 -m 780000 7FFFFF 8 -ob -o List/BANKED.s19 List/$(PROJEKT_NAME).s19
here is the Error:
SRecCvt v1.0.26 Converting S-Record File: List/Gallenschuetz.s19 S2060F8000C000AA Error:(9) S-Record Data Not In Specified Memory Map
the s19file is shown like:
S01900004C6973742F47616C6C656E7363687565747A2E783132B9 S2060F8000C000AA S2247EC0000A722004F62004C10A2609CC04001662CF7920040A1D21431FFC21418C000A2572 S2247EC020081C2143011879214118722141FC213F8C003225081C2143021879213F187221B0 S2247EC0403FFC213D8C006425081C2143041879213D1872213DFC213B8C03E825081C2143D0 S2247EC060081879213B1872213BFC21398C177025081C2143101879213918722139CC0001A0 S2247EC0801662CF0A1C0002401D0000400A0A0AF62005260B1C000040C6017B200520071DA0 S2137EC0A0000040792005F60000C4407B21460A4A S2247F4000CF3FFF180BFD0016180B200011180BFF0030CEC104ED31A63427372A021A02857D S2247F4020602604ED1E20F034972B10B764A31EEE1C180A703004B4F93020DCEC1E3B180D62 S2247F40401B0010EE1CE670186B30AD8025F7303020C5CE2137C720026C318E2E6625F9180C ... ... ...
concerning the memory Error in the CRC function:
I have tried it both with the paged and global adress an no one works
/// Flash Start Adresse //#define FLASH_START_ADDR 0x00FB8000 // paged #define FLASH_START_ADDR 0x007EC000 // global /// Flash End Adresse //#define FLASH_END_ADDR 0x00FBBFFF // paged #define FLASH_END_ADDR 0x007EFFFF // global
and the function is:
void Flash_CalcCRC(void) { // Puffer Zeiger auf aktuelles Byte mit Startadresse initialisieren // for paged addressing //static T_UC08* pucBuffer = (T_UC08*) FLASH_START_ADDR; // for global addressing static T_UC08 *_atfar pucBuffer = (T_UC08 *_atfar) FLASH_START_ADDR; // calculate only a part of flash T_UI16 uiBytesCounter = 0; // Temp Var T_UI16 uiCryptPos = 0; // calculate just 64 bytes every time and go out from function for (ulNumLoops ; (ulNumLoops <= FLASH_END_ADDR) && (uiBytesCounter < 64 ); ulNumLoops++) { // increment counter uiBytesCounter++; // copy Word from buffer in uiCryptPos uiCryptPos = (T_UI16) *pucBuffer; // increment buffer pointer pucBuffer++; // EXOR with retrun CRC uiCryptPos ^= uiFlashCRC16; // calc CryptArrays uiFlashCRC16 = *(T_UI16*)(uiCRC16l + (uiCryptPos & 0x000F)) ^ *(T_UI16*)(uiCRC16h + ((uiCryptPos & 0x00F0) >> 4)) ^ (uiFlashCRC16 >> 8); } if ( ulNumLoops == FLASH_END_ADDR ) { ucFinishFlag = 1; Flash_SetCRC16(uiFlashCRC16); } }
now if I debug the function in the codewarior with iondart one
it shown, that he is taking the content of the address 0L
I m sorry for posting this, I m a very beginner with embedded systems and S12X, this is my first experience with it.
I m still trying and serching in google and this forum!!
thanks soo much friends
Hi,
global addresses in Cosmic require the modifier @gpage, you can try something like this:
/* gpage pointer allows accessing any area of global map, paged and non paged */
@far @gpage unsigned int uiMP @0x00FB8000;
@far @gpage unsigned int *puiMP;
*puiMP = &uiMP;
while (puiMP < (@far @gpage unsigned int*) 0x00FBBFFF)
{
uiCryptPos = *puiMP;
/* Here you calculate your CRC and then increment the pointer */
puiMP ++;
}
I hope it works.
I can't help you with Cosmic. CrasyCat suggestion works in CodeWarrior.
Regarding SrecCvt error.
S2060F8000C000AA
Highlighted address doesn't fit global memory range specified in sreccvt -m switch -m 780000 7FFFFF.
Global 0F8000 points to RAM, not flash. Do you have some initialized variable in "far" RAM? Maybe Cosmic doesn't support initialization of far variables and puts them directly to S-records?
ups sorry I sended you the not banked s19 File!
sorry sorry
here the command:
CHEX_OUT_MOT = -o List/$(PROJEKT_NAME).s19..$(LINK) $(LDFLAGS) -o List/$(PROJEKT_NAME).x12 $(LINKFILE)$(S19) -s $(CHEX_OPT_MOT) $(CHEX_OUT_MOT) List/$(PROJEKT_NAME).x12
this is not a big problem, because the not banked S19 file is not needed, only the banked is needed
so the error is not critical
the error happens when I add the @far pointer
no I dont have any initialized variables in RAM
I will send an email direktly to Cosmic, and post the response here
thank you Kef for answer! I m still looking for a solution
I got it!!!!!
const _atfar @gpage T_UC08* pucBuffer = (const _atfar @gpage T_UC08 *) FLASH_START_ADDR;
and it works fine!!
thanks for help friends!
and have a nice day,night!!
now I m really stumped
I change the line to T_UI16
static T_UI16 *_atfar pucBuffer = (T_UI16 *_atfar) FLASH_START_ADDR;
and now I read the adress 4000L, see codewarior2.jpg
Sorry friends, if I m taking your time, I hope I can help you too in the future