S12UB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12UB

3,989 Views
trav
Contributor III
We're using the S12UB boards in my microcontroller class, are these boards still avaiable?  I noticed no suppliers seem to have them, and freescale doesn't have a direct buy for it.

If they are not, is there a new board to use?


These boards have been a pain to get setup, even my Professor who has proabably been on the HC11's since they came out is having a tough time with the new S12UB board.
Labels (1)
0 Kudos
Reply
4 Replies

1,211 Views
Lundin
Senior Contributor IV
Google is your friend. Google for "S12UB" revealed this Freescale link as hit no 3:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=LFEBS12UB

Judging from that link, Freescale do sell them directly for $85. Freescale part is "LFEBS12UB".
0 Kudos
Reply

1,211 Views
JimDon
Senior Contributor III
For what ever reason, they don't seem to be available. No distributors are showing stock, and when I try buy direct, it gets an error.

You could look in to the Dragon12 or MiniDragon12 here.
0 Kudos
Reply

1,211 Views
Alban
Senior Contributor II
Hello Trav,

What is a S12UB board ???
What does it look like and what is the exact reference ?
All FSL boards have a reference.

Cheers,
Alban.
0 Kudos
Reply

1,211 Views
trav
Contributor III
Ok there must have been something wrong with the ordering system when I tried, because it would error out, now it's working.
0 Kudos
Reply