Routing of power to 9S12XEQ512 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Routing of power to 9S12XEQ512 MCU

2,304 Views
vpapakos
Contributor I

Dears,

Recently we decided to redesign the PCB of one of our products that uses 9S12XEQ512 MCU. 

On the datasheet, the power input to the voltage regulator is pin 31 VDDR.

Based on this, on the old version of the PCB, the central power connection is on PIN 31 like on picture old.jpg. The Ground polygon pour below the processor connects to the ground plane at one location on VSS2 pin through single via. The ground plane is directly below the top layer. But this is not according to the recommendations of page 1263.

On refererence manual page 1263 Appendix C PCB Layout Guidelines there are the following suggestions

Central point of the ground star should be the VSS3 pin. (pin 32)

Central power input should be fed in at the VDDA/VSSA pins. (pins 59 & 62)

Is the existing PCB routing for power and Ground considered satisfactory and robust for ESD purposes? 

Why is the recommendation for central power connection at VDDA VSSA and not to the Voltage Regulator pin VDDR? Is it to reduce the noise on the analog domain only, or it affects EMC/ESD performance as well?

Finally if the central power connection return is VSSA, then where should the Ground plane be connected? At VSS3 or VSSA?

Please have a look at the new proposed routing at new.jpg. In the second image, 3V is not routed below the IC, and power is routed from VSSA and VDDA pin and not VDDR pin. The supply to VDDR has to pass through two vias to reach there. Ground connection to Ground plane is near VSS3.Bottom layer parts are connted to 3V before the main ground connection. Should the main ground also be directly connected to pin 62 ( I added resistor footprint for this), or is it ok to use the ground plane only?

Are there any advantages to this approach? Will it have optimal ESD performance? Or should we keep the old routing which we already know has no problems with ESD discharges?

Best Regards,

0 Kudos
Reply
2 Replies

2,137 Views
dastek
Contributor III

Hi,

What package are you using.

I use a LQFP-112 which is the same core, but pin 31 is my Port B7.

I have 3 x 220nF caps that decouple the internal 2.5V supply.  They decouple an internal regulator.

I have 3 of these connected to VDD CORE, VDDF and VDD PLL.

From my experience connect all VSS pins (VSS1, VSS2, VSS3, VSSA, VSSR, VSSPLL, VSSX) to the GND plane as close to the pin as possible.

Use more than one via if there is space as this reduces inductance.

 

That's my 5c worth.

Regards,

Wade

 

0 Kudos
Reply

2,259 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @vpapakos,

I'm sorry but layout review are out of scope of our technical support.

But the idea is to decouple the analog and the digital circuits so that the noise in the analog part is reduced.

The purpose of the star is to have one central point (vias to the GND plane) and this should be near the crystal so that the traces of the crystal can be as short as possible.

 

Regards,

Daniel

0 Kudos
Reply