Regarding number of timer zero channels available for 48 pin ZVM16 MCU.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding number of timer zero channels available for 48 pin ZVM16 MCU.

954 Views
pratibhasurabhi
Contributor V

Hi,

I want to know the number of timer zero channels in ZVM16(48 pin) MCU.

In Pin out diagram of ZVM16(48 pin) MCU only one channel is shown as below in yellow mark,

pastedImage_3.png

I want to confirm, is there only one channel of timer zero or other channels are there?

Its urgent,please inform me the answer of same as early as possible.

Thanks.

0 Kudos
Reply
2 Replies

813 Views
RadekS
NXP Employee
NXP Employee

Hi Pratibha,

It seems that you probably have some older version of reference manual.

The current version 2.11 shows also routing option for IOC0_1 and IOC0_2 at pins PS0 and PS1.

S12ZVMpinoutLQFP48.png

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

813 Views
pratibhasurabhi
Contributor V

Thank you Radek for quick reply!

0 Kudos
Reply