Reg. MC9S12DJ64 Controller - EEPROM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reg. MC9S12DJ64 Controller - EEPROM

3,736 次查看
balajiprabhakar
Contributor I
Hi,
 
I need to know a small information about the MC9S12DJ64 controller.
 
What is the endurance/life cycle of the EEPROM in the IC? For how many cycles the EEPROM can be used, is it 10,000 or more than that.
 
Please clarify the same.
 
regards,
 
Balaji.
标签 (1)
0 项奖励
回复
6 回复数

1,605 次查看
balajiprabhakar
Contributor I
Hi all,
 
Can I get the complete datasheet, with all reference documents in the same datasheet for MC9S12DJ64. If it is available please do attach the link for me....
 
 
regards,
 
Balaji.
0 项奖励
回复

1,605 次查看
JimDon
Senior Contributor III
Sorry, but the HCS12 documentation is not all in one document.

Hopefully Freescale will never do thing this way again, but for now that is how it is down.

Here is a link to all the data sheets.
This is a zip file with them all.
0 项奖励
回复

1,605 次查看
balajiprabhakar
Contributor I
Thanks Jim for the zip file.
 
Can you please tell me how many erase/write cycles be performed on the EEPROM in MC9S12DJ64.
 
with regards,
 
Balaji.
 
 
0 项奖励
回复

1,605 次查看
JimDon
Senior Contributor III
Well Freescale eeprom is normally rated at 300K Typical, given a normal temperature range.
I
0 项奖励
回复

1,605 次查看
balajiprabhakar
Contributor I
Hi Jim,
 
The EEPROM which you have mentioned above, is that a seperate EEPROM IC you are telling about, or the EEPROM in the controller.
 
I want to clarify this because when I go for a seperate IC for EEPROM, then I will get the typical 300k. But what about the EEPROM that is inbuilt in the controller.
 
Do I get the same 300k. I think it will be definitely less than 300k, say around 10k to 100k.
 
Please clarify me on this.
 
with regards,
 
Balaji.
0 项奖励
回复

1,605 次查看
JimDon
Senior Contributor III
Now, how would I know about any external EEPROM you might be thinking of using.

I am referring to the internal EEPROM.
The Flash is good to 100K.
0 项奖励
回复