Question about bandgap voltage of S12Z internal voltage regulator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about bandgap voltage of S12Z internal voltage regulator

Jump to solution
1,154 Views
Snaku
Contributor III

Hi,

There is a figure (Figure A-1 Current Injection on GPIO Port if Vin > VDDX) in the S12ZVC user manual, it shows there is a VBG and comparator in the voltage regulator, but I want to know the resistors value and when the P2 MOS will open or close.
Thank you,Snaku

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,016 Views
RadekS
NXP Employee
NXP Employee

Hi Snaku,

The scheme of Voltage Regulator at Figure A-1 is not the real circuit of the internal voltage regulator. It is a just very simplified version for indication of internal voltage regulator functionality.

Therefore, we cannot specify the resistor values.

The P2 work on continues conduction mode – it is not a switch. The P2 regulates their current for achieving stabilized 5V at VDDX line.

The Voltage regulator specifications are in chapter E.1 VREG Electrical Specifications (page 725, RM Rev1.3).

Despite in fact that the scheme of Voltage Regulator at Figure A-1 is simplified, it nicely shows potential issue with Injection currents and MCU in STOP mode. When Iin>Iload, the internal voltage regulator is not able to keep 5V at output VDDX line. So, we have to manage that Iload will be always higher than Iin – for example by adding some external resistor between VDDX and GND or by disconnection of Iin current source….


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,017 Views
RadekS
NXP Employee
NXP Employee

Hi Snaku,

The scheme of Voltage Regulator at Figure A-1 is not the real circuit of the internal voltage regulator. It is a just very simplified version for indication of internal voltage regulator functionality.

Therefore, we cannot specify the resistor values.

The P2 work on continues conduction mode – it is not a switch. The P2 regulates their current for achieving stabilized 5V at VDDX line.

The Voltage regulator specifications are in chapter E.1 VREG Electrical Specifications (page 725, RM Rev1.3).

Despite in fact that the scheme of Voltage Regulator at Figure A-1 is simplified, it nicely shows potential issue with Injection currents and MCU in STOP mode. When Iin>Iload, the internal voltage regulator is not able to keep 5V at output VDDX line. So, we have to manage that Iload will be always higher than Iin – for example by adding some external resistor between VDDX and GND or by disconnection of Iin current source….


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply