Problem connecting to HCS12X board using a Processor Expert project through serial monitor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem connecting to HCS12X board using a Processor Expert project through serial monitor

1,267 次查看
Mounties
Contributor I

We are encountering errors when debugging.  We're only using the asynchronous bean, AS1-AnsynchroSerial.  The error generated is "CommError: 00000008 =  CE_FRAME; InQue: 5, OutQue: 0".  Any ideas as to what may be causing this or typical scenarios that generate this error?

标签 (1)
0 项奖励
回复
1 回复

882 次查看
Mounties
Contributor I

We are pretty sure that the problem are based on the CPU settings and we're wondering if anyone knows the correct CPU settings for ProcessorExpert to work?

0 项奖励
回复