Hi,
According to the reference manual (page 35), memory region 0x4000->0x7FFF of the 9S12XEP100 is Unpaged FLASH. I am using the region 0x5000->0x7FFF to store 'const' read-only data.
The memory region is programmed OK by the BDM, along with the code which is in 0xC000->0xFFFF. When the processor is reset the debugger shows the region 0x5000->0x7FFF is filled with the right values.
But, if the software is started then halted, the region 0x5000->0x7FFF shows different (wrong) values.
What could be causing this? The software uses the small memory model and I thought in this memory model 0x4000->0x7FFF will always access the same region as it's an un-paged area?
Thanks, Ian
Hi,
I just checked and it looks like that bit is set.
There is legacy code that uses the FLASH in region 0x4000->0x4FFF and I assumed it was accessed through the local address space.
Maybe this is not the case and I will try and find out.
Thanks, Ian
So this explains why you can't read data in 0x4000.
ROMHM=1 - Disables access to the Flash or ROM in the lower half of the memory map (0x4000-0x7FFF).These physical locations of the Flash or ROM can still be accessed through the program page window. Accesses to 0x4000–0x7FFF will be
mapped to 0x14_4000-0x14_7FFF in the global memory space (external access).