PC-Lint Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PC-Lint Tool

2,315 次查看
dorin75
Contributor I
Hi !
 
I'm working with the CW 5.7.0 and my target is a MC9S12XDP512 (starterkit from SofTec). I want to compile/link my project with PC-Lint but I dont't have one. Somebody knows where I could download that PC-Lint from ? 
 
Thank you in advance,
Dorin
标签 (1)
0 项奖励
回复
2 回复数

1,100 次查看
J2MEJediMaster
Specialist I
I'm puzzled as to your version of CodeWarrior. The reason I wonder is two fold: first, if you're developing for the HC12SX series (I'm working on with MC9S12XDT512 myself), the latest version of Codewarrior is 4.5. Second, when you use the CW 4.5 Wizard to build the project, it offers to set the the project up for PC-lint. So, you should be able to use PC-lint through using of the setup wizard.

However, I'll have to emphasize that as a moderator, I have the deluxe software installation. :smileyhappy: You'll have to purchase PC-lint from Gimpbel software. If you do, then Codewarrior integrates with it well through its setup wizard.

---Tom

Message Edited by J2MEJediMaster on 2006-09-08 10:01 AM

0 项奖励
回复

1,100 次查看
DanielM
Contributor III
Hi,

as far as I know PC-Lint is a comercial product by Gimpel Software (http://www.gimpel.com/). You will have to buy it from them.

Daniel
0 项奖励
回复