[P-Flash] Erase and Write to PFlash will occur ILLEGAL_BP in MC9S12XS128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[P-Flash] Erase and Write to PFlash will occur ILLEGAL_BP in MC9S12XS128

Jump to solution
1,074 Views
Pogo
Contributor III

I've tried to erase and write data to PFlash, but it will occur ILLEGAL_BP. The following list is my test environment.


MCU: MC9S12XS128

IDE : CodeWarrior IDE version 5.9.0 Build 2836

BDM: TBDML

 

Here is my Code

void PFlash_Write(word *ptr){    unsigned char i;    while((FSTAT & FSTAT_CCIF_MASK) == 0);  //wait if command in progress    FSTAT = 0x30;       //clear ACCERR and PVIOL    FCCOBIX = 0x00;    FCCOB = 0x067E;     //program 0x7E0000    FCCOBIX = 0x01;    FCCOB = 0x0000;    for(i=2; i<6; i++)  //fill data (4 words) to FCCOB register    {        FCCOBIX = i;        FCCOB = *ptr;        ptr++;    }    FSTAT = 0x80;       //launch command    while((FSTAT & FSTAT_CCIF_MASK) == 0);  //wait for done}/******************************************************************************/void PFlash_Erase(void){    while((FSTAT & FSTAT_CCIF_MASK) == 0);  //wait if command in progress    FSTAT = 0x30;       //clear ACCERR and PVIOL    FCCOBIX = 0x00;    FCCOB = 0x0A7E;     //erase 0x7E0000    FCCOBIX = 0x01;    FCCOB = 0x0000;    FSTAT = 0x80;       //launch command    while((FSTAT & FSTAT_CCIF_MASK) == 0);  //wait for done}void main{    unsigned short u16Data[4];    for( ;     {        ....        if( getkey() == 'w' )        {            u16Data[0] = 100;            u16Data[1] = 110;            u16Data[2] = 120;            u16Data[3] = 130;            DisableInterrupts;            PFlash_Erase();            PFlash_Write(u16Data);            EnableInterrupts;        }    }}

 Could you have any suggestion for me to solve this problem? Thanks a lot.

 

 

Regards,

Pogo

Labels (1)
0 Kudos
1 Solution
633 Views
kef
Specialist I

In the code:

 

#pragma CODE_SEG __NEAR_SEG ramcodeseg
static void executeflashcmd(void)
{
   asm
   {
      PSHC             // remember I-bit state
      SEI              // disable interrupts
   }
   FSTAT = 0x80;       //launch command
   while((FSTAT & FSTAT_CCIF_MASK) == 0);  //wait for done

   asm PULC;           // restore I-bit
}
#pragma CODE_SEG DEFAULT

  

In PRM file you need to add following line into PLACEMENT block

      ramcodeseg        INTO RAM;
 

To make it working you need to use ANSI C startup routine, which will copy routine from flash to RAM at startup. Else you will need to copy routine by your own code.

View solution in original post

0 Kudos
4 Replies
633 Views
kef
Specialist I

It is because flash memory is not readable while any flash command is being executed (flash/erase/etc). This part of your code should execute from RAM:

 

    FSTAT = 0x80;       //launch command
    while((FSTAT & FSTAT_CCIF_MASK) == 0);  //wait for done
 

Also, since interrupts can happen at any time, even while writing/erasing flash, you also need to disable interrupts before launching flash command. (It is possible to move critical ISR's and interrupt vectors table to RAM and disable only less time critical interrupts).

0 Kudos
633 Views
Pogo
Contributor III

Thanks for your reply.

Could you show me how to copy the code into RAM as function and how to call it?

I use the same code to erase or program D-Flash, but it doesn't have this issue.

Thanks again.

 

Regards,

Pogo

0 Kudos
634 Views
kef
Specialist I

In the code:

 

#pragma CODE_SEG __NEAR_SEG ramcodeseg
static void executeflashcmd(void)
{
   asm
   {
      PSHC             // remember I-bit state
      SEI              // disable interrupts
   }
   FSTAT = 0x80;       //launch command
   while((FSTAT & FSTAT_CCIF_MASK) == 0);  //wait for done

   asm PULC;           // restore I-bit
}
#pragma CODE_SEG DEFAULT

  

In PRM file you need to add following line into PLACEMENT block

      ramcodeseg        INTO RAM;
 

To make it working you need to use ANSI C startup routine, which will copy routine from flash to RAM at startup. Else you will need to copy routine by your own code.

0 Kudos
633 Views
Pogo
Contributor III

Hi Kef,

It works fine.

Thanks for your help.

 

 

Regards,

Pogo

0 Kudos