Need information Regarding CAN interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need information Regarding CAN interface

976 次查看
pratayay123
Contributor III

Dear Team,

I Need the below information Regarding the CAN transceiver for MTRCKTSPNZVM128  (MC9S12ZVML128 MCU).

1.  Is there an Inbuild CAN transceiver is available for the MTRCKTSPNZVM128 development kit(MC9S12ZVML128 MCU).

2. is there any process document or workshop/tutorial available for CAN protocol for the MTRCKTSPNZVM128 development kit(MC9S12ZVML128 MCU).

3. If the inbuild CAN transceiver is not available in kit then what is the process to connect CAN for the MTRCKTSPNZVM128 development kit(MC9S12ZVML128 MCU).

4. Please share supporting documents for CAN protocol for NXP

 

Thanks,

Pratyay

0 项奖励
回复
1 回复

925 次查看
StanoA
NXP TechSupport
NXP TechSupport

Hello Pratayay,

There is the CAN driver IC on board connected to J8.
You can use the AN:
https://www.nxp.com/docs/en/application-note/AN4975.pdf
and CAN Protocol Standard:
https://www.nxp.com/docs/en/reference-manual/BCANPSV2.pdf
and attached SW example with calculators to build your application.
I think it could help you with your task.

Best Regards,

Stano.

0 项奖励
回复