NEED HELP: I can not set any mode in MC9S12XHZ512

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NEED HELP: I can not set any mode in MC9S12XHZ512

875 次查看
OldDeng
Contributor I

as the title, when i want to set the MC9S12XHZ512 to mode "Emulation Expanded", the pin MODEB is always low. Even i connect this pin to VCC whit a 4.7k resistance, it dosen't work. I have no choice but to find help here. If anyone can give me some advice, whether it uesful or not, thanks a lot

标签 (1)
0 项奖励
回复
1 回复

656 次查看
kef
Specialist I

Could you explain what for do you need emulation expanded mode for?

 

You pulled MODB high, but MODB is low. This can be so if 1) on PCB MODB is connected directly to VSS, 2) MCU is executing some program that makes MODB pin driven low, 3) MODB pin is damaged, 4) different packages have different pinouts. Are you sure you are pulling MODB pin high?

0 项奖励
回复