Hi Ladislav,
Thanks again for taking the time to answer my question. Yes, I can fit what I need into near Flash. (Unpaged Flash?)
My code is from $C000 to $D8F2, 6,226 bytes by my reckoning. It may expand in future but not much. The only time this code is changed is when I do a code revision, it never gets changed on the fly.
My configurable constants are from $4000 to $424C (588 bytes) They may expand in future but certainly never anywhere near $4FFF. (4,095 bytes maximum available, I think.)
In my program the configurable constants from $4000 to $424 C are copied to RAM at start up where the program accesses them. They can be modified there and burnt back to Flash in the program if necessary.
Does that answer your question?
Regards,
Robert
Reqards,
Robert