Hello Everyone,
I'm just starting off some work with the S12 series, specifically the DJ256. I am working out the memory mapping for the RAM, EE, and Registers.
Would someone with some more experience be able to comment if anything looks out of place?
My tentative configuration is:
INITEE 0x01 EEPROM mapped to 0x0000 - 0x0xFFF (4kB) and enabled
INITRM 0x39 RAM mapped to 0x1000 - 0x3FFF (12kB) and high-aligned
INITRG 0x40 Registers mapped to 0x4000 - 0x4800 (2kB)
Does this look okay? Is there a better configuration? And lastly, am I correct that the ROMHM bit in the MISC register should
be left at its default (unset, lower-half EE/ROM can be accessed)? I'd appreciate any help, thanks!
Adam
Hi,
Once I remapped the memory in bellow mentioned way. Your approach is good because it takes only 2KB from nonpaged memory 4000. My approach takes 4KB from this memory because I placed an EEPROM there. Moreover, I would like to present some facts to be taken into account in the CodeWarrior environment.
Some comments to your setup:
OK; INITEE 0x01 EEPROM mapped to 0x0000 - 0x0xFFF (4kB) and enabled
OK; INITRM 0x39 RAM mapped to 0x1000 - 0x3FFF (12kB) and high-aligned ( first block selected, up alligned)
comment: the same is INITRM 0x01 RAM mapped to any 16 k block 0x1000 - 0x3FFF (12kB) and high-aligned
OK; INITRG 0x40 Registers mapped to 0x4000 - 0x4800 (2kB) 0x4000 - 0x43FF
comment: the RAM occupies only 1K so it is mapped at 0x4000 - 0x43FF
The project representing my setup is attached. It is made for the compatible MCU with the same memory map. The main facts are highlighted bellow.
1) main.c module
//The Memory is remapped in following way
//
//- Registers : 0000~03FF
//- RAM : 1000~3FFF
//- EEPROM : 4000~4FFF
//- Unpaged flash : 5000~7FFF, C000~FFFF
//- Paged flash : 0x(30~3F)(8000~BFFF)
//
//Remapping is made in the file Start12.c before Init() function is called.
//(Init() function is automatically generated by CodeWarrior to initialize variables)
//
//
// //-----------------------------------
// folowing lines are placed inside Start12.c to define memory map (line 413)
// *(unsigned char*)0x11 = 0x00; // INITRG = 0x00; Set the Reg map position 0x0000~0x03FF
// asm nop; // recommended
// *(unsigned char*)0x10 = 0x01; // INITRM = 0x01; Set the RAM map position 0x1000~0x3FFF
// *(unsigned char*)0x12 = 0x41; // INITEE = 0x41; Set the EEPROM map position 0x4000~0x4FFF, EEON=1
// //------------------------------------
//
// Also *.prm file must be adjusted to meet these changes. (See line 11 and 18 in the prm file)
2) PRM file lines 11-18:
__EXTERN_C void _Startup(void) {
#endif
/* purpose: 1) initialize the stack
2) initialize the RAM, copy down init data etc (Init)
3) call main;
parameters: NONE
called from: _PRESTART-code generated by the Linker
or directly referenced by the reset vector */
*(unsigned char*)0x11 = 0x00; // INITRG = 0x00; Set the Reg map position 0x0000~0x03FF
asm nop; // recommended
*(unsigned char*)0x10 = 0x01; // INITRM = 0x01; Set the RAM map position 0x1000~0x3FFF
*(unsigned char*)0x12 = 0x41; // INITEE = 0x41; Set the EEPROM map position 0x4000~0x4FFF, EEON=1
3) PRM file changes:
/* Register space */
/* IO_SEG = PAGED 0x0000 TO 0x03FF; intentionally not defined */
/* EPROM */
// EEPROM = READ_ONLY 0x0400 TO 0x0FEF;
EEPROM = READ_ONLY 0x4000 TO 0x4FEF;
/* RAM */
RAM = READ_WRITE 0x1000 TO 0x3FFF;
/* non-paged FLASHs */
// ROM_4000 = READ_ONLY 0x4000 TO 0x7FFF;
ROM_4000 = READ_ONLY 0x5000 TO 0x7FFF;
Please look into attachment to check it.
Best regards,
Ladislav