Max voltage can be applied for BLDC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max voltage can be applied for BLDC

930 Views
miko7895
Contributor I

Hello;

i am using MC9s12ZVMx12EVB and using the example for BLDC motor control with the freeMaster (BLDC sensorless) described in AN4704.

the motor runs with no problem, i need to know the max voltage can be applied on the board as i need to operate BLDC with voltage 48V

if the board can operate do i need to change in the software?

0 Kudos
Reply
1 Reply

826 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

MagniV MCUs target 12V automotive applications.

The the following application notes discuss MagniV in 24V and 48V applications.

AN11967 S12ZVM Family in 48 V Applications 

AN5082 MagniV in 24V Applications

Regards,

Daniel