Mapping PIT hardware trigger signals - Can't find the SoC Guide for xep processor.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mapping PIT hardware trigger signals - Can't find the SoC Guide for xep processor.

2,140件の閲覧回数
Pedro_
Contributor III
Hi all,
 
The s12xep100 Reference Manual mentions 8 hardware trigger lines in the PIT module.
The System on Chip Guide should detail which peripheral modules are mapped to this lines, however, I haven't been able to find this guide.
 
Do you know if that document is available?
 
Thanks again.
Pedro.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

985件の閲覧回数
Steve
NXP Employee
NXP Employee
The "SoC guide" is actually chapter one of the manual. You'll find the details of the use of the PIT as a hardware trigger there but it's written from the point of view of the peripheral rather than the PIT (actually the ATD peripherals).
0 件の賞賛
返信

985件の閲覧回数
Pedro_
Contributor III
That answers my question, Steve, thanks.
 
I am falling short with the max. underflow time for the ECT Modulus Down Counter and I was wondering if I could latch the accumulators using those triggers .. It was a long shot anyway.
 
I could always force latch (ICLAT) from the PIT interrupt vector, but then I have to consider if latancy is going to be an issue for me.
 
mm .. I need etpus !!
 
Thanks again
0 件の賞賛
返信