MagniV S12ZVC Operate at 15V?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MagniV S12ZVC Operate at 15V?

862件の閲覧回数
Derrick
NXP Employee
NXP Employee

Can the VLG-MC9S12ZVC evaluation board operate from a 15V power supply?

 

I believe that the MCU can run from 15V (is that true?), but is there anything on the evaluation board that would prevent this?  Or are there any other cautions to consider if operating from 15V?

 

Best Regards,

Derrick

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

745件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Derrick,

sorry for delay.

I checked schematic and I do not see any problem with 15V.

The lowest limit is given by MCU (the standard operational range up to 18V, but it will survive 40V for short time) and Buzzer (operational range up to 20V). All other limits are above…


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

745件の閲覧回数
Derrick
NXP Employee
NXP Employee

Hello?  Is anyone looking into this?

0 件の賞賛
返信