MagniV S12ZVC Operate at 15V?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MagniV S12ZVC Operate at 15V?

844 Views
Derrick
NXP Employee
NXP Employee

Can the VLG-MC9S12ZVC evaluation board operate from a 15V power supply?

 

I believe that the MCU can run from 15V (is that true?), but is there anything on the evaluation board that would prevent this?  Or are there any other cautions to consider if operating from 15V?

 

Best Regards,

Derrick

Labels (1)
0 Kudos
Reply
2 Replies

727 Views
RadekS
NXP Employee
NXP Employee

Hi Derrick,

sorry for delay.

I checked schematic and I do not see any problem with 15V.

The lowest limit is given by MCU (the standard operational range up to 18V, but it will survive 40V for short time) and Buzzer (operational range up to 20V). All other limits are above…


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

727 Views
Derrick
NXP Employee
NXP Employee

Hello?  Is anyone looking into this?

0 Kudos
Reply