MSCAN Module for MC9S12XEQ512 MAL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MSCAN Module for MC9S12XEQ512 MAL

3,365 次查看
mohamedbouich01
NXP Employee
NXP Employee

Hi,

I would like to use the MC9S12XEQ512MAL to generate a CAN frame (without receive one). Indeed I have to to wake up an IC with a specific CAN frame.

I made several try without success......

I don't have the frame expected at MCU pin number 104 (txcan0).

 

Would like, please, help me on this issue ? Maybe you have a code ready to use to obtain the CAN frame with this version of S12X.

 

Many thanks.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

3,235 次查看
RadekS
NXP Employee
NXP Employee

Hi Mohamed,

The simple example code is in attachment.

More examples are for example here:

LAMA's S12XE unofficial examples

The “official” msCAN driver:

http://www.nxp.com/files/microcontrollers/software/device_drivers/MSCAN_S12_DEVD.zip


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复