MM9Z1J638(Error launchinq xxx FLASH PnE U-MultiLink)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1J638(Error launchinq xxx FLASH PnE U-MultiLink)

588 Views
jylpbdl
Contributor I

I am using MM9Z1J638 MCU, but there is a fast chip seems to be debugged by me, under the same environment another development board can enter debugging, but this one can not, how to unlock the chip?(cw 10.7)

  • The following is the error promotion

Conficm
Device is secure. Erase to unsecure?
No
Yes

"Launchinq xxx FLASH PnEU-MultiLink'has
encountered a problem. Wouild you like to
export diagnosticinformation and send it to
Freescale?
Error launchinq E245 FLASH PnE U-MultiLink


The target MCUis notresponding
Please turn MCU power off (Under 0.1v,
turn MCU power on, and then clickOK.
This will attempt to enter debug mode
througha power on reset sequenCe.

0 Kudos
Reply
3 Replies

423 Views
peter_pinewski
NXP Employee
NXP Employee

Hi @jylpbdl , @cui1 ,

I just ran across this.  I am assuming that you have RESETA and RESET tied together.  Please note that flashing problems can occur when these pins are connected.  A simple solution is to provide a 470nF capacitor at these reset pins to ground.  This should allow you to program.

peter_pinewski_0-1708540108293.png

 

Regards,

Peter

 

0 Kudos
Reply

527 Views
cui1
Contributor II
Hello jylpbdl
I have the same problem as you. Have you solved it? Could you let me know if it is resolved
0 Kudos
Reply

525 Views
jylpbdl
Contributor I

remain to be solved

0 Kudos
Reply