MM9Z1J638 Demo Software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1J638 Demo Software

4,508 Views
rdrosescu
Contributor III

Hi,

I tried to download MM9Z1J638 Demo Software for RD9Z1-638-12V-C (MM9Z1J638-DEMO-APPSW). The indicated link is no longer accessible.

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=MM9Z1J638-DEMO-APPSW&appType=file1&DOWNL...

Error message:
This site can’t be reached
The webpage at https://cache.nxp.com/secured/assets/downloads/en/apps/MM9Z1J638-Demo-APPSW.zip?__gda__=1632855104_c... permanently. web address.
I reported more but nothing has changed (for the better).

Thanks!

Radu

0 Kudos
Reply
9 Replies

4,490 Views
StanoA
NXP TechSupport
NXP TechSupport

Hi Radu,

Sorry for the inconvenience, the software pack is attached. We will try to correct this as soon as possible.

The attachment is divided into two consecutive send parts due to attachment space capacity.

Thanks for understanding.

Best Regards,

Stano.

0 Kudos
Reply

4,487 Views
StanoA
NXP TechSupport
NXP TechSupport

Second part. Please unpack and rename it to *.001  resp *.crc.

0 Kudos
Reply

4,479 Views
rdrosescu
Contributor III

Hi Stano,

Thank you for your answer. Unfortunately the first file is corrupted and after being repaired with WinRAR it generates a 638_drv_lib folder, which does not contain all the files needed for a complete CW project. The second archive appears to contain an antlr folder with a PythonCodeGenerator.class file and a CRC.
It is not clear whether the renaming * .001 means MM9Z1J638-Demo-APPSW.002, and * .crc means MM9Z1J638-Demo-APPSW.crc. Who is in this case MM9Z1J638-Demo-APPSW.001? And how can they be merged together in one MM9Z1J638-Demo-APPSW.zip file? In fact I only need RD9Z1_638_12VLA_CAN_demo code warrior project to run with RD9Z1-638-12V-C evaluation board as specified in KTRD9Z1-638-12V-CUG.
Best regards,
Radu
0 Kudos
Reply

4,469 Views
StanoA
NXP TechSupport
NXP TechSupport

The second file.

0 Kudos
Reply

4,470 Views
StanoA
NXP TechSupport
NXP TechSupport

Hi Radu,

Sorry for the troubles. I attached it once again – the files are two time packed. I will send it in two phases again.

They are multiple zip files. Inside the unpacked 638_drv_lib folder is the “src” folder which contains the CW project files, also the project you are looking for.

I hope it could help you in your task.

Best Regards,

Stano.

0 Kudos
Reply

4,441 Views
rdrosescu
Contributor III

Hi Stano,

Now it is OK.I really appreciate your support. I would have one last question. I have all three evaluation modules with MM9Z1J638: RD9Z1-638-12V (LIN), RD9Z1-638-12VC (CAN) both for PbA Batteries and RD9Z1-638-4Li for Li-Ion. All have a program preinstalled in SOC flash memory. In 2016, when I purchased the modules, CW projects were also available for these pre-installed programs, respectively RD9Z1-638-12V-APPSP with RD9Z1-638-12V (LIN), RD9Z1-638-4Li-SW_Rel1.03 with RD9Z1-638-4Li and KT9Z1 -638-REFAPP for the evaluation kit KIT9Z1J638EVM. All differ from demo variants in MM9Z1J638 Demo Software.zip. For example RD9Z1_638_12VLA_LIN_demo differs from the flash program ie RD9Z1-638-12V-APPSP, the same for Li-Ion.
The CAN variant - RD9Z1-638-12VC did not have a CW project associated with the flash program. Is there such a project? Is it somehow called KT9Z1_638_CAN_demo that comes with MM9Z1J638 Demo Software, or are there differences in this case as well?

Thanks!

Radu

0 Kudos
Reply

4,423 Views
StanoA
NXP TechSupport
NXP TechSupport

Hi Radu,

The example projects are in the previous sent *.zip pack also on web:

https://www.nxp.com/webapp/Download?colCode=MM9Z1J638-DEMO-APPSW&appType=license

here inside:

…\MM9Z1J638\MM9Z1J638-Demo-APPSW.zip\638_drv_lib\build\cw\638\

There is also the “make_cw_project.exe” file on:

…\MM9Z1J638\MM9Z1J638-Demo-APPSW.zip\638_drv_lib\drv\project\638\

I hope it can help you in your task.

Best Regards,

Stano.

0 Kudos
Reply

4,407 Views
radudrosescu
Contributor III

Thanks. I consider this case solved.

Radu

0 Kudos
Reply

4,401 Views
StanoA
NXP TechSupport
NXP TechSupport

Thanks for message Radu, you are welcome.

Stano.

0 Kudos
Reply