MCS9S12G STOP mode current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCS9S12G STOP mode current

跳至解决方案
1,427 次查看
wenfengyao
Contributor II

When I use this chip, after entering the STOP mode, the current consumption is 2mA, and the unused IO ports have also entered the pull-up input mode. Is there any way to reduce power consumption?

0 项奖励
回复
1 解答
1,411 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

The device is CMOS technology device so in full stop mode there is no reason for an additional current. Except, if there are some „sources“/grounds connected via pins to ground/„sources“. In this case you have to think how to avoid this additional consumption ( for example; lighting diode either switched to gnd or Vdd, sensor, input of another device)
The question is also where you measure the consumption.
Is your mode full stop .... is everything switched off? (Pseudo stop mode)

Best regards,

Ladislav

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,412 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

The device is CMOS technology device so in full stop mode there is no reason for an additional current. Except, if there are some „sources“/grounds connected via pins to ground/„sources“. In this case you have to think how to avoid this additional consumption ( for example; lighting diode either switched to gnd or Vdd, sensor, input of another device)
The question is also where you measure the consumption.
Is your mode full stop .... is everything switched off? (Pseudo stop mode)

Best regards,

Ladislav

0 项奖励
回复