MCS9S12G STOP mode current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCS9S12G STOP mode current

ソリューションへジャンプ
1,883件の閲覧回数
wenfengyao
Contributor II

When I use this chip, after entering the STOP mode, the current consumption is 2mA, and the unused IO ports have also entered the pull-up input mode. Is there any way to reduce power consumption?

0 件の賞賛
返信
1 解決策
1,867件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

The device is CMOS technology device so in full stop mode there is no reason for an additional current. Except, if there are some „sources“/grounds connected via pins to ground/„sources“. In this case you have to think how to avoid this additional consumption ( for example; lighting diode either switched to gnd or Vdd, sensor, input of another device)
The question is also where you measure the consumption.
Is your mode full stop .... is everything switched off? (Pseudo stop mode)

Best regards,

Ladislav

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,868件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

The device is CMOS technology device so in full stop mode there is no reason for an additional current. Except, if there are some „sources“/grounds connected via pins to ground/„sources“. In this case you have to think how to avoid this additional consumption ( for example; lighting diode either switched to gnd or Vdd, sensor, input of another device)
The question is also where you measure the consumption.
Is your mode full stop .... is everything switched off? (Pseudo stop mode)

Best regards,

Ladislav

0 件の賞賛
返信