MC9S12XEP100 programming and de-bugging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S12XEP100 programming and de-bugging

1,671 次查看
roberthiebert
Senior Contributor I

I am working on  a hobby project using the MC9S12XEP100, programming in assembler and using Code Warrior 5.9.0 Special Edition. I'm not clear on just what hardware I need to buy to connect to the processor to download the S19 file and de-bug the program using CW. I can't justify spending a lot of money on additional hardware so what is my lowest cost solution to this?

0 项奖励
回复
2 回复数

1,660 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

I suppose you do not use any of our development boards which contains programing/debugging interface populated on the board. Moreover, I suppose you will not require stand-alone programming used in manufacturing process in the future.

The only thing you need is USB Multilink Universal from Pemicro.

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320168&productTab=1

One more thing I would like to suggest you is to download Unsecure_12 from www.pemicro.com download area. The tool unsecures the MCU when you accidentally secure it. Of course, the CodeWarrior is able also to unsecure but, from my experience, sometime it fails and Unsecure_12 is able to do it better.

 

Best regards,

Ladislav

0 项奖励
回复

1,654 次查看
roberthiebert
Senior Contributor I

Thanks for that information

Regards,

Robert

0 项奖励
回复