Hello Darshan,
If you use 10-bit resolution, as Kef suggested, this will result in a resolution of 4.88mV, or slightly less than 0.5 degree.
If you then wished to adjust the resolution to exactly 0.5 degree C, to simplify the calculation process, you could place a resistive voltage divider between the temperature sensor and the ATD input. This might consist of a 820 ohm series resistor, and a 33k shunt resistor, and would provide a voltage change of 9.76mV per degree C at the ATD input.
Regards,
Mac